• NIBCO Announces New Tailpiece Product Launch

    • Press Tailpiece
    2019-03-21

    ELKHART, Ind. — (March 20, 2019) NIBCO INC. is proud to announce the launch of our new tailpiece (PC634) pipe joining component. This product is designed for use in multiple applications which include connecting to inlets or outlets for plumbing and mixing stations used to regulate radiant heating supply water temperatures.

     

    “This launch continues our commitment to ongoing product development to help contractors and homeowners take advantage of high-quality products and over 100 years of innovation in the joining industry,” said Marilyn Morgan, Senior Product Manager. “The PC634 tailpieces are a superior choice for pipe joining in heating systems as well as baseboard and fan coil applications.”

     

    Other applications for the tailpieces include use with mixing valves, diverting valves and other plumbing devices or equipment in potable water and heating systems requiring a straight thread union connection.

     

    NIBCO press fittings are made with 100% North American pure copper which is a premium, proven and preferred material for plumbing and mechanical applications. Manufactured in our Stuart’s Draft, Virginia facility, the tailpieces are convenient to use and part of our commitment to high-quality flow control products and manufacturing services.

     

    Tailpieces (PC634) are third party certified to ASME B16.51, UPC and PS-117.

     

    About NIBCO INC.

    Founded in 1904, NIBCO INC. is a leading provider of valves, fittings and flow control products for commercial, industrial and institutional construction as well as residential and irrigation markets. NIBCO is headquartered in Elkhart, Ind., and has 10 manufacturing plants located throughout the United States, Mexico and Poland. Visit NIBCO.com for information on the complete line of NIBCO products.

  • News

    • New NIBCO Press Slip Ball Valve Simplifies Installation

      9/24/2019 12:00:00 AM

      New NIBCO Press Slip Ball Valve Simplifies Installation 2019-09-24   ELKHART, Ind. — (September 24, 2019) NIBCO INC. continues to expand its press valve line with the Press Slip Ball Valve (PC-FP600A-S-LF). This valve is easy to add to existing copper piping, or to replace an old valve without needing e

    • NIBCO Announces New Tailpiece Product Launch

      3/21/2019 12:00:00 AM

      NIBCO Announces New Tailpiece Product Launch 2019-03-21 ELKHART, Ind. — (March 20, 2019) NIBCO INC. is proud to announce the launch of our new tailpiece (PC634) pipe joining component. This product is designed for use in multiple applications which include connecting to inlets or outlets for plumbing a

    • NIBCO Announces New Product Launch: Press Extended Repair Couplings

      3/21/2019 12:00:00 AM

      NIBCO Announces New Product Launch: Press Extended Repair Couplings 2019-03-21 ELKHART, Ind. — (March 20, 2019) NIBCO INC. is proud to announce the launch of our press extended repair couplings (PC601L). These new couplings are specifically designed for pipe repair in plumbing, mechanical and hydronic