• NIBCO Launches FLO-BOSSTM, a New Line of Balancing Valves

    • FLO-BOSS
    2016-11-17
    ELKHART, IND. – (November 14, 2016) NIBCO INC. proudly announces the launch of its rebranded and expanded line of balancing valves: FLO-BOSSTM. The extended line of balancing valves advances the company’s offering with additions such as the new press ends, valves with ultra-flow and low-flow flexibility, and a variety of accessory items.

    “FLO-BOSS represents the next evolution of balancing valves,” stated Tim Burnette, General Manager Controls. “We have engineered a collection of new products to meet our customer’s needs, like the press balancing system. These products are installed in factory, tested in factory, and shipped as finished goods. Our growing selection is the right fit for just about any type of project, and comes from the most reliable name in flow control.”

    The press balancing system allows users to install balancing valves up to 95% faster and flame-free, offering a safer alternative to soldering. The secure, consistent, and leak-proof connection is a smooth and efficient process that works perfectly with the lightweight, ergonomic NIBCO® press tool. All FLO-BOSS valves are quality tested to meet stringent NIBCO specifications and are backed by a five-year, 125% limited warranty.

    If you would like to learn more about the new and exciting line of FLO-BOSS balancing valves, a comprehensive price booklet can be found at www.nibco.com/floboss.

    About NIBCO INC.
    Founded in 1904, NIBCO INC. is a leading provider of valves, fittings and flow control products for commercial, industrial and institutional construction as well as residential and irrigation markets. NIBCO is headquartered in Elkhart, IN, and has 11 distribution and manufacturing plants located throughout the United States, Mexico and Poland. Visit NIBCO.com for information on the complete line of NIBCO products.
    • FLO-BOSS
  • News

    • NIBCO purchases warehouse/distribution building in Virginia

      8/15/2018 12:00:00 AM

      NIBCO purchases warehouse/distribution building in Virginia 2018-08-15  ELKHART, IND. — (August 15, 2018) NIBCO INC. has announced the purchase of a 173,000-square-foot building in Buena Vista, Virginia. The facility, which is approximately 30 miles from the NIBCO INC. Stuarts Draft, Va., wrot copper ma

    • WROT ACR Fittings UL Recognized to 700 PSI

      2/16/2017 12:00:00 AM

       ELKHART, INDIANA – (February 16, 2017) – NIBCO INC. is proud to announce that a select assortment of WROT ACR fittings are now UL Recognized to 700 PSI. These products have been tested to the UL 207 performance requirements.