• News

    • NIBCO purchases warehouse/distribution building in Virginia

      8/15/2018 12:00:00 AM

      NIBCO purchases warehouse/distribution building in Virginia 2018-08-15  ELKHART, IND. — (August 15, 2018) NIBCO INC. has announced the purchase of a 173,000-square-foot building in Buena Vista, Virginia. The facility, which is approximately 30 miles from the NIBCO INC. Stuarts Draft, Va., wrot copper ma

    • WROT ACR Fittings UL Recognized to 700 PSI

      2/16/2017 12:00:00 AM

       ELKHART, INDIANA – (February 16, 2017) – NIBCO INC. is proud to announce that a select assortment of WROT ACR fittings are now UL Recognized to 700 PSI. These products have been tested to the UL 207 performance requirements.