• IAPD Convention & Expo

    Location: Chicago, IL
    Start Date: 2017-10-16
    End Date: 2017-10-19


    Chemtrol, a brand of NIBCO is exhibiting at IAPD in booth #205 on October 19 in Chicago, IL.

    Media Contact:
    pr@nibco.com
  • News

    • NIBCO Introduces PERTpro™ Tubing to its Flexible Piping System Line

      3/2/2017 12:00:00 AM

      NIBCO Introduces PERTpro™ Tubing to its Flexible Piping System Line 2017-03-02 ELKHART, INDIANA – (March 2, 2017) – NIBCO INC. is proud to announce the introduction of PERTpro™ flexible tubing for potable water plumbing and barrier tubing for hydronics and radiant heating. A unique combinat

    • WROT ACR Fittings UL Recognized to 700 PSI

      2/16/2017 12:00:00 AM

       ELKHART, INDIANA – (February 16, 2017) – NIBCO INC. is proud to announce that a select assortment of WROT ACR fittings are now UL Recognized to 700 PSI. These products have been tested to the UL 207 performance requirements.

    • NIBCO Launches Press Extended Adapters

      2/1/2017 12:00:00 AM

      ELKHART, IND. – (February 1, 2017) NIBCO INC. proudly announces the launch of its new Press System Extended Adapters. These new adapters are longer than the standard WROT adapters and have been specifically designed to ensure they have the necessary length for a Press crimp.